:WMEMory:PATTern:FILE:GCODe
Command Syntax
:WMEMoryN:PATTern:FILE:GCODe {ON | OFF | 1 | 0}
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:PATTern:FILE:GCODe?
Query Response
{1 | 0}
Description
When you have specified a PAM4 signal type (see :WMEMory:SIGNal:TYPE), this command lets you specify whether symbols are Gray Coded or uncoded. When patterns are specified (see :WMEMory:PATTern:FILE:NAME), the pattern must match this selection.