:WMEMory:INTerpolate:FACTor
Command Syntax
:WMEMoryN:INTerpolate:FACTor <factor>
<factor> is an integer.
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMoryN:INTerpolate:FACTor?
Description
For the selected waveform memory, this command specifies a factor (integer value) that determines the number of interpolated points Infiniium between sampled points in the input waveform. To select the interpolation on load method, use the :WMEMory:INTerpolate:METHod command.