:WMEMory:INTerpolate:METHod

Command Syntax

:WMEMoryN:INTerpolate:METHod {NONE| SINC}

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Syntax

:WMEMoryN:INTerpolate:METHod?

Description

For the specified waveform memory's interpolation on load setting, this command selects sin(x)/x interpolation or no interpolation.

SINC
Selects the sin(x)/x method, which is the default and is preferred when reconstructing a signal (having evenly spaced samples) that has been band limited. The number of points in the output waveform are evenly spaced and are set by the interpolation factor (:WMEMory:INTerpolate:FACTor) command.
NONE
Turns interpolation on load off.