:WMEMory:INTerpolate:STATus:REASon?
Query Syntax
:WMEMoryN:INTerpolate:STATus:REASon?
Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.
Query Response
<string>
Description
If the status of the specified waveform memory's interpolation on load is invalid (see :WMEMory:INTerpolate:STATus?), this query returns a description of the invalid status.
If the status of the specified waveform memory interpolation on load is correct, this query returns an empty string.