:WMEMory:INTerpolate:STATus?

Query Syntax

:WMEMoryN:INTerpolate:STATus?

Where N identifies one of eight {1:8} possible waveform memories. For example, :WMEMory4.

Query Response

{CORR | INV}

Description

Returns the status of the specified waveform memory's interpolation on load. The following responses can be returned:

CORR
The memory location contains correctly interpolated waveform data.
INV
The interpolation on load for the specified memory location is invalid. To query the reason for the invalid status, use the :WMEMory:INTerpolate:STATus:REASon? query.