:CRECovery:LBWMode
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CRECovery{1:8}:LBWMode {FIXed | RDEPendent}
Where the {1:8} specifier identifies a slot number which is associated with clock recovery module. On 86108A modules, specify slot 1.
Query Syntax
:CRECovery{1:8}:LBWMode?
Description
Sets the module's loop-bandwidth entry mode.
- FIXed
- Specifies a fixed loop bandwidth. Enter the actual bandwidth using the
:CRECovery{1:4}CLBandwidthcommand. - RDEPendent
- Specifies a rate-dependent loop bandwidth. The loop bandwidth is indirectly set by dividing the data rate (
:CRECovery{1:4}CRATecommand) by the data-rate divide ratio (:CRECovery{1:4}RDIVidercommand). The loop bandwidth can not be entered when the module is in this mode.
Command Compatibility
- 86108A/B
- 83496A/B Option 300
Example Command Sequence
:CRECovery1:LBWMode FIXed :CRECovery1:LBANdwidth BW300KHZ