:HISTogram:ASCii:DATA?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:HISTogram{1:4}:ASCii:DATA?
Where the {1:4} specifier identifies one of four possible histograms. For example, :HISTogram3.
Description
Returns the histogram database as ASCII data (comma-separated values). Each value provides the number of counts for each point in the histogram. To query the number of points (comma-separated values), use the :HISTogram:POINts? query. To return the data in binary, use the :HISTogram:INTeger:DATA? query.