:HISTogram:WINDow:BORDer
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:HISTogram{1:4}:WINDow:BORDer {ON | OFF | 1 | 0}
Where the {1:4} specifier identifies one of four possible histograms. For example, :HISTogram3.
Query Syntax
:HISTogram{1:4}:WINDow:BORDer?
Query Response
{1 | 0}
Description
Displays (ON) or hides (OFF) the solid-line histogram window border. The border allows you to view which region of the measurement database is used to construct the histogram. The border does not have to be displayed to create a histogram. By default, the border is off. The histogram must be enabled prior to enabling the histogram window border.