:HISTogram:SOURce
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:HISTogram{1:4}:SOURce <source_waveform>
Where the {1:4} specifier identifies one of four possible histograms. For example, :HISTogram3.
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}DIFF{1:4}CGMemory{1:8}FUNCtion{1:16}
Query Syntax
:HISTogram{1:4}:SOURce?
Description
Selects the source waveform for the indicated histogram. The histogram window will track the source's vertical and horizontal scale.