:HISTogram:WINDow:DEFault
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:HISTogram{1:4}:WINDow:DEFault
This command supports the DEFault common child command.
Where the {1:4} specifier identifies one of four possible histograms. For example, :HISTogram3.
Description
Sets the X1, X2, Y1, and Y2 coordinates to time and amplitude values required to create a centered histogram window 8 major graticule divisions wide and 6 divisions high. The window is shown as a blue border line on the display. This default window is the same shape regardless of the type of histogram specified with the :HISTogram:AXIS command. The histogram window defines the region of the measurement database that is used to construct the histogram. Use the :HISTogram:X and :HISTogram:Y commands to create a custom window.
Default Histogram Window