:HISTogram:INCRement?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:HISTogram{1:4}:INCRement?
Where the {1:4} specifier identifies one of four possible histograms. For example, :HISTogram3.
Description
Queries the amplitude or time spacing between the points in the histogram. For vertical (left and right) histograms, this is the amplitude spacing between the points are along the vertical axis. For horizontal (top and bottom) histograms, this is the time spacing between the points along the horizontal axis. Use the :HISTogram:POINts? query to return the number of points in the histogram. To return the actual counts for each point, use the :HISTogram:ASCii:DATA? or :HISTogram:INTeger:DATA? queries.
Vertical Histogram (LEFT)
Horizontal Histogram (BOTTom)