:HISTogram:AXIS
Command Syntax
:HISTogram{1:4}:AXIS {LEFT | RIGHt | BOTTom | TOP}
Where the {1:4} specifier identifies one of four possible histograms. For example, :HISTogram3.
Query Syntax
:HISTogram{1:4}:AXIS?
Description
Selects the orientation of the histogram. Select LEFT or RIGHt for vertical histograms (voltage or power measurements). Select TOP or BOTTom for horizontal histograms (timing measurements). Histograms are displayed as a series of lines (vertical or horizontal). The length of each line represents the number of hits of data on that row (or column) of the display. In vertical histograms with LEFT placement, zero hits correspond to the left edge of the graticule. In horizontal histograms with BOTTom placement, zero hits correspond to the bottom edge of the graticule.
To set the X-axis size of vertical histograms, use the :HISTogram:VSIZe command. To set the Y-axis size of horizontal histograms, use the :HISTogram:HSIZe command.
Vertical Histogram (LEFT)
Horizontal Histogram (BOTTom)