:HISTogram:ORIGin?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:HISTogram{1:4}:ORIGin?
Where the {1:4} specifier identifies one of four possible histograms. For example, :HISTogram3.
Description
Returns the origin of the histogram's border, which is the region of the database that is used to calculate the histogram results. For left or right histograms, the origin is equal to the border's bottom edge and is the same value as :HISTogram:WINDow:Y1 setting. For top and bottom histograms, the origin is equal to the border's left edge and is the same value as :HISTogram:WINDow:X1 setting. Use the :HISTogram:AXIS command to select a left, right, top, or bottom histogram placement.