:JDMemory:CLEar
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Command Syntax
:JDMemory{1}:CLEar
Where the {1} is the required specifier that indicates that only one jitter data memory is available at this time, :JDMemory1.
Description
Clears the Jitter data memory.
Requires FlexDCA revision A.05.70 and above.