:JDMemory:CWINdow
Command Syntax
:JDMemory{1}:CWINdow TIMe{1}
Where the {1} is the required specifier that indicates that only one jitter data memory is available at this time, :JDMemory1.
Query Syntax
:JDMemory{1}:CWINdow?
Description
The :JDMemory{1}:CWINdow command allows you to assign a jitter data memory waveform to a Waveform content window. Since there is only one window available at this time, there is currently no selection to make with this command.
As of this release, there is only one Waveform content window, so you will not need to use this command.
In future revisions, the :JDMemory{1}:CWINdow command will select a content window in which to display a jitter data memory waveform. In FlexDCA, four different types of content windows exist: Waveform (TIMe1), Group Delay (GDELay), Magnitude (MAGNitude), and Phase (PHASe). Each type varies by its type of X- and Y-axis units. Any given waveform is only compatible with one of these four content window types. Therefore, FlexDCA automatically assigns waveforms to the proper type of content window, such as Waveform or Phase. Waveforms can not be assigned to a different type of content window. For example, a Waveform waveform can not be moved to or shown in a Magnitude content window.
| Argument | Displayed Waveform Content Window |
Number of Available Windows |
Scale Units | |
|---|---|---|---|---|
| Programmatically | Via Front Panel |
|||
| TIMe1 | Waveform | 1 | 1 | Y-Axis: Volts or Watts (linear scale) X-Axis: seconds |
Requires FlexDCA revision A.03.00 and above.