:JDMemory:LOAD
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Command Syntax
:JDMemory{1}:LOAD
Where the {1} is the required specifier that indicates that only one jitter data memory is available at this time, :JDMemory1.
Description
Loads the currently displayed jitter data into jitter memory. Use the :JDMemory:LOAD:SOURce command to select the source, for example channel 1A. Use the :JDMemory:DISPLay command to display graphs and scalar data from the jitter memory.
To load a jitter database file into jitter memory, use the :JDMemory:FILE:LOAD and :JDMemory:FILE:NAME commands.
Requires FlexDCA revision A.05.70 and above.
Example Command Sequence
:JDMemory1:LOAD:SOURce CHAN1A :JDMemory1:LOAD :JDMemory1:DISPLay ON
Child Commands
:SOURcespecifies the source waveform on which to perform the measurement.