:JDMemory:DSTatus:REASon?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Query Syntax
:JDMemory{1}:DSTatus:REASon?
Where the {1} is the required specifier that indicates that only one jitter data memory is available at this time, :JDMemory1.
Query Response
<string>
Description
Returns a description of the status of the specified Jitter Data memory. If an jitter data is currently in the specified Jitter Data memory location, the name of the source waveform will be returned. For example, "Source: Channel 1A". If the Jitter Data memory is empty, the string "Please select a file." is returned. If the file is corrupt or an incorrect type, the string "Unable to load file." is returned. To check the status of the Jitter Data memory, use the :JDMemory:DSTatus? parent query.
Requires FlexDCA revision A.05.70 and above.