:JDMemory:LOAD:SOURce
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Command Syntax
:JDMemory{1}:LOAD:SOURce <source_waveform>
Where the {1} is the required specifier that indicates that only one jitter data memory is available at this time, :JDMemory1.
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}DIFF{1:4}FUNCtion{1:16}
Query Syntax
:JDMemory{1}:LOAD:SOURce?
Query Response
<source_waveform>
Description
Specifies the source waveform for the currently displayed jitter data that will be loaded into jitter data memory using the command.:JDMemory:LOAD
Requires FlexDCA revision A.05.70 and above.