:JDMemory:DSTatus?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Query Syntax
:JDMemory{1}:DSTatus?
Where the {1} is the required specifier that indicates that only one jitter data memory is available at this time, :JDMemory1.
Query Response
{CORR | INV}
Description
Returns the status of the specified Jitter Data memory. To query the reason for the current state of the memory, use the :JDMemory:DSTatus:REASon? query. The following responses can be returned:
CORR- The Jitter Data memory location contains jitter data. To clear memory, use the
:JDMemory:CLEarcommand. INV- The Jitter Data memory location does not contain jitter data.
Requires FlexDCA revision A.05.70 and above.