:JDMemory Subsystem
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
The jitter data memory subsystem commands allow you to use jitter data offline. Only available in Jitter Mode, jitter data memory can be saved, recalled, displayed, and measured. There is only one jitter data memory, and it is identified by the integer "1" in :JDMemory1. Only files saved using the internal format (.jdx) can be imported into Jitter Mode's jitter data memory.
To load currently displayed jitter data into jitter memory using the :JDMemory:LOAD command. To use Jitter Spectrum Analysis (JSA) memory, use the :JSAMemory subsystem. To save Jitter data to a file, use the :DISK:JDATabase:SAVE command.