:LTESt:LLINe:SWAVeform:CMODe:STATe
Instrument:
N1010A
N1000A
Meas. mode:
TDR
Flex Apps:
FlexDCA
This command is compatible with TDR/TDT mode only.
Command Syntax
:LTESt:LLINe:SWAVeform:CMODe{1:8}{A|C}:STATe {DISK | MEMory | OFF}
Where the specifier {1:8}{A|C} identifies a common-mode channel.
Query Syntax
:LTESt:LLINe:SWAVeform:CMODe{1:8}{A|C}:STATe?
Description
In TDR/TDT Mode, specifies the reporting action for the selected common-mode waveforms upon completion of limit testing for a limit line test. Use the command argument to select or turn off the reporting action. To disable the reporting action of all channel, common-mode, differential, and function waveforms, use the :LTEST:LLINe:SWAVeform:RESet command.
To turn on limit testing for a limit line test, use the :LTESt:LLINe:TEST:STATe command.
| Argument | Description |
|---|---|
| DISK | Saves the waveform to a file (.wfmx) in the %USER_DATA_DIR%\Limit Lines folder. Use the :LTESt:LLINe:SWAVeform:CMODe:FNAMe command to specify the file name. |
| MEMory | Saves the waveform to a memory location. Use the :LTESt:LLINe:SWAVeform:CMODe:WMEMory command to specify the memory location. |
| OFF | Turns off the saving of a common-mode waveform. |
Requires FlexDCA revision A.04.50 and above.
Example Command
:LTESt:LLINe:SWAVeform:CMODe2A:STATe DISK