:LTESt:LLINe:SWAVeform:CMODe:WMEMory
Instrument:
N1010A
N1000A
Meas. mode:
TDR
Flex Apps:
FlexDCA
This command is compatible with TDR/TDT mode only.
Command Syntax
:LTESt:LLINe:SWAVeform:CMODe{1:8}{A|C}:WMEMory WMEMory{1:8}
Where the specifier {1:8}{A|C} identifies a common-mode channel.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:LLINe:SWAVeform:CMODe{1:8}{A|C}:WMEMory?
Description
Upon completion of limit testing for a limit line test, any common-mode waveform can be automatically saved to one of eight available waveform memory locations. Use this command to associate a specific waveform memory to a specific wommon-mode waveform. To actually enable common-mode waveforms to be saved, use the :LTESt:LLINe:SWAVeform:CMODe:STATe command.
To enable limit testing for a limit line test, use the :LTESt:LLINe:TEST:STATe command.
Requires FlexDCA revision A.04.00 and above.
Example
:LTESt:LLINe:SWAVeform:CMODe2A:WMEMory WMEMory3