:LTESt:LLINe:SWAVeform:CHANnel:WMEMory
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:LLINe:SWAVeform:CHANnel{1:8}{A|B|C|D}:WMEMory WMEMory{1:8}
Where the specifier {1:8}{A|B|C|D} identifies the channel.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:LLINe:SWAVeform:CHANnel{1:8}{A|B|C|D}:WMEMory?
Description
Upon completion of limit testing for a limit line test, any channel waveform can be automatically saved to one of eight available waveform memory locations. Use this command to associate a specific waveform memory to a specific channel. To actually enable channel waveforms to be saved, use the :LTESt:LLINe:SWAVeform:CHANnel:STATe command.
To enable limit testing for a limit line test, use the :LTESt:LLINe:TEST:STATe command.
Requires FlexDCA revision A.04.50 and above.
Example
:LTESt:LLINe:SWAVeform:CHANnel2A:WMEMory WMEMory3