:LTESt:LLINe:SWAVeform:FUNCtion:WMEMory
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:LLINe:SWAVeform:FUNCtion{1:64}:WMEMory WMEMory{1:8}
Where {1:64} identifies a function.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:LLINe:SWAVeform:FUNCtion{1:64}:WMEMory?
Description
Upon completion of limit testing for a limit line test, any function waveform can be automatically saved to one of eight available waveform memory locations. Use this command to associate a specific waveform memory to a specific function waveform. To actually enable function waveforms to be saved, use the :LTESt:LLINe:SWAVeform:FUNCtion:STATe command.
To enable limit testing for a limit line test, use the :LTESt:LLINe:TEST:STATe command.
Example
:LTESt:LLINe:SWAVeform:FUNCtion2:WMEMory WMEMory3