:LTESt:LLINe:SWAVeform:DIFF:STATe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:LLINe:SWAVeform:DIFF{1:8}{A|C}:STATe {DISK | MEMory | OFF}
Where {1:8}{A|C} identifies a differential channel.
Query Syntax
:LTESt:LLINe:SWAVeform:DIFF{1:8}{A|C}:STATe?
Description
Specifies the reporting action for the selected differential waveform upon completion of limit testing for a limit line test. Use the command argument to select or turn off the reporting action. To disable the reporting action of all channel, common-mode, differential, and function waveforms, use the :LTEST:LLINe:SWAVeform:RESet command.
To turn on limit testing for a limit line test, use the :LTESt:LLINe:TEST:STATe command.
| Argument | Description |
|---|---|
| DISK | Saves the waveform to a file (.wfmx) in the %USER_DATA_DIR%\Limit Lines folder. Use the :LTESt:LLINe:SWAVeform:DIFF:FNAMe command to specify the file name. |
| MEMory | Saves the waveform to a memory location. Use the :LTESt:LLINe:SWAVeform:DIFF:WMEMory command to specify the memory location. |
| OFF | Turns off the saving of a differential waveform. |
Requires FlexDCA revision A.04.50 and above.
:SYSTem:MODE OSCilloscope :CHANnel1A:DISPlay ON :CHANnel1B:DISPlay ON :TRIGger:PLOCk ON :DIFF1A:DMODe ON :SYSTem:AUToscale // Load and start limit line test. :LLINe1:LOAD:FNAMe "%USER_DATA_DIR%\Limit Lines\Golden Test.lltx" :LLINe1:SOURce DIFF1A :LLINe1:DISPlay ON // Display first limit line test.// Configure "Save Differential Waveform" reporting. :LTESt:LLINe:SWAVeform:RESet // Turn saving of all waveforms off. :LTESt:LLINe:SWAVeform:DIFF1A:FNAMe "%USER_DATA_DIR%\Waveforms\FailDiffWaveform.wfmx" // Waveform file name. :LTESt:LLINe:SWAVeform:DIFF1A:STATe DISK // Save waveform to file.// Run limit testing. :LTESt:LLINe:TEST1:MODe SOFailure // Stop limit testing on fail condition. :LTESt:LLINe:TEST1:STATe ON // Enable limit testing. :ACQuire:STOP :ACQuire:CDISplay // Clear existing waveform data. :ACQuire:RUN // Enable data acquisition.