:LTESt:LLINe:SWAVeform:FUNCtion:FNAMe
Command Syntax
:LTESt:LLINe:SWAVeform:FUNCtion{1:64}:FNAMe "<path substitution string>\subfolder\filename"
Where {1:64} identifies a function.
Where <path substitution string> is a string that expands into a specific file path. For example, %USER_DATA_DIR%.
Where "subfolder" is an optional path folder. For example, %USER_DATA_DIR%\Waveforms.
Where "filename" is a string without the filename extension.
Query Syntax
:LTESt:LLINe:SWAVeform:FUNCtion{1:64}:FNAMe?
Description
Upon completion of limit testing for a limit line test, any function waveform can be automatically saved to a file. Use this command to enter a file name and path for the selected function. The file name extension (.wfmx) is automatically appended to the file name. To actually enable function waveforms to be saved, use the :LTESt:LLINe:SWAVeform:FUNCtion:STATe command. To enable testing limits on a limit line test, use the :LTESt:LLINe:TEST:STATe command. This command supports the DEFault common child command.
Do not include an extension when specifying the filename.
The default folder for storing function waveform files is in %USER_DATA_DIR%\Waveforms as shown in this pictures. It is good practice to include a path substitution string with the filename. For example, %USER_DATA_DIR%\Waveforms\filename.
File names must include a path when using the child :FNAMe command. The :FNAMe command is not affected by a Default Setup or Factory Preset.
Specifying a path using a path substitution string in the filename ensures that the file will be saved in (or loaded from) the standard user-data folder. Failure to use a path substitution string may result either in a file created in an parent folder or a file error.
Requires FlexDCA revision A.04.50 and above.
Example Command
:LTESt:LLINe:SWAVeform:FUNCtion4:FNAMe "DUT132"