:LTESt:LLINe:SWAVeform:CHANnel:STATe
Command Syntax
:LTESt:LLINe:SWAVeform:CHANnel{1:8}{A|B|C|D}:STATe {DISK | MEMory | OFF}
Where the specifier {1:8}{A|B|C|D} identifies the channel.
Query Syntax
:LTESt:LLINe:SWAVeform:CHANnel{1:8}{A|B|C|D}:STATe?
Description
Specifies the reporting action for the selected channel waveform upon completion of limit testing for a limit line test. Use the command argument to select or turn off the reporting action. To disable the reporting action of all channel, common-mode, differential, and function waveforms, use the :LTEST:LLINe:SWAVeform:RESet command.
To turn on limit testing for a limit line test, use the :LTESt:LLINe:TEST:STATe command.
| Argument | Description |
|---|---|
| DISK | Saves the waveform to a file (.wfmx) in the %USER_DATA_DIR%\Limit Lines folder. Use the :LTESt:LLINe:SWAVeform:CHANnel:FNAMe command to specify the file name. |
| MEMory | Saves the waveform to a memory location. Use the :LTESt:LLINe:SWAVeform:CHANnel:WMEMory command to specify the memory location. |
| OFF | Turns off the saving of a channel waveform. |
Requires FlexDCA revision A.04.50 and above.
Example
This example shows the general steps required to load two limit line tests. One test is for a channel waveform and one test is for a function waveform. Limit testing is applied to each limit line test and both waveforms are saved to a file upon test completion which occurs on the first failed data point. The waveform content window is tiled so that the two waveforms do not overlap. In a real example, you would need to create the limit test for your waveforms and manage the correct positioning of the limit lines.
:SYSTem:MODE OSCilloscope :CHANnel1A:DISPlay ON :FUNCtion1:DISPlay ON :TRIGger:PLOCk ON :SYSTem:AUToscale // Load and start two limit line tests. :LLINe1:LOAD:FNAMe "%USER_DATA_DIR%\Limit Lines\Golden Test.lltx" :LLINe1:SOURce CHANnel1A :LLINe1:DISPlay ON // Display first limit line test. :LLINe2:LOAD:FNAMe "%USER_DATA_DIR%\Limit Lines\Golden Test.lltx" :LLINe2:SOURce FUNCtion1 :LLINe2:DISPlay ON // Display second limit line test. :DISPlay:WINDow:TIME1:DMODe STILed // Stack and tile waveform window.// Configure "Save Channel Waveform" reporting. :LTESt:LLINe:SWAVeform:RESet // Turn saving of all waveforms off. :LTESt:LLINe:SWAVeform:CHANnel1A:FNAMe "%USER_DATA_DIR%\Waveforms\FailCH1A.wfmx" // Waveform file name. :LTESt:LLINe:SWAVeform:CHANnel1A:STATe DISK // Save waveform to file.// Configure "Save Function Waveform" reporting. :LTESt:LLINe:SWAVeform:FUNCtion1:FNAMe "%USER_DATA_DIR%\Waveforms\FailFunction1.wfmx" // Waveform file name. :LTESt:LLINe:SWAVeform:FUNCtion1:STATe DISK // Save waveform to file.// Run limit testing. :LTESt:LLINe:TEST1:MODe SOFailure // Stop limit testing on fail condition. :LTESt:LLINe:TEST1:STATe ON // Enable limit testing. :LTESt:LLINe:TEST2:MODe SOFailure // Stop limit testing on fail condition. :LTESt:LLINe:TEST2:STATe ON // Enable limit testing. :ACQuire:STOP :ACQuire:CDISplay // Clear existing waveform data. :ACQuire:RUN // Enable data acquisition.