:LTESt:LLINe:SWAVeform:DIFF:WMEMory
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:LLINe:SWAVeform:DIFF{1:8}{A|C}:WMEMory WMEMory{1:8}
Where {1:8}{A|C} identifies a differential channel.
Where the argument WMEMory{1:8} identifies a waveform memory.
Query Syntax
:LTESt:LLINe:SWAVeform:DIFF{1:8}{A|C}:WMEMory?
Description
Upon completion of limit testing for a limit line test, any differential waveform can be automatically saved to one of eight available waveform memory locations. Use this command to associate a specific waveform memory to a specific differential waveform. To actually enable differential waveforms to be saved, use the :LTESt:LLINe:SWAVeform:DIFF:STATe command.
To enable limit testing for a limit line test, use the :LTESt:LLINe:TEST:STATe command.
Example
:LTESt:LLINe:SWAVeform:DIFF2A:WMEMory WMEMory3