:SOURce:AMPLitude
Command Syntax
:SOURce{1:8}{A|B|C|D}:AMPLitude <amplitude>
Where the {1:8}{A|B|C|D} specifier identifies a module's channel.
Where <amplitude> is a double.
Query Syntax
:SOURce{1:8}{A|B|C|D}:AMPLitude?
Description
On Arbitrary Waveform Generator (AWG) and simulated extended modules, sets the specified waveform's amplitude. Enter the amplitude in volts for electrical channels and Watts for optical channels. To set the offset, use the :SOURce:OFFSet command.
Requires FlexDCA revision A.02.00 and above for simulated extended modules. Revision A.06.00 and above for AWG extended modules.
Selecting AWG Channels
When sending a :SOURce subsystem command to an AWG, the method used to specify the AWG's channel may look confusing at first glance. This is because, the AWG's front-panel channels are labeled 1, 2, 3, and 4, but FlexDCA identifies channels with letters (A, B, C, or D). As a result, you must convert the AWG's channel number to an equivalent FlexDCA letter as shown in this table. For example, to enable channel 3 of an AWG that is installed in FlexDCA's slot 5 use the following command: :SOURce5C:AMPLitude 1.2E-1.
| AWG Channel |
Equivalent Letter |
|---|---|
| 1 | A |
| 2 | B |
| 3 | C |
| 4 | D |
Example Command
:SOURce3A:AMPLitude 1.2E-1