:SOURce:FOTWo:JITTer
Command Syntax
:SOURce{1:8}{A|B|C|D}:FOTWo:JITTer <jitter>
Where the {1:8}{A|B|C|D} specifier identifies a module's channel.
Where <jitter> is a double.
Query Syntax
:SOURce{1:8}{A|B|C|D}:FOTWo:JITTer?
Description
Sets the amount of F/2 jitter, in unit intervals (UI), that is added to the selected simulated waveform. The default value is 10 mUI. Use the :SOURCe:FOTWo:STATe command to turn apply or disable this jitter.
Example Command Sequence
:SOURCe5A:FOTWo:JITTer: 1.5E-2 :SOURCe5A:FOTWo:STATe ON
Requires FlexDCA revision A.04.50 and above.
| AWG Channel |
Equivalent Letter |
|---|---|
| 1 | A |
| 2 | B |
| 3 | C |
| 4 | D |
Selecting AWG Channels
When sending a :SOURce subsystem command to an AWG, the method used to specify the AWG's channel may look confusing at first glance. This is because, the AWG's front-panel channels are labeled 1, 2, 3, and 4, but FlexDCA identifies channels with letters (A, B, C, or D). As a result, you must convert the AWG's channel number to an equivalent FlexDCA letter. For example, to enable channel 3 of an AWG that is installed in FlexDCA's slot 5 use the following command: :SOURce5C:OENable ON.