:SOURce:NOISe:RN
Source:
Simulate
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SOURce{1:8}{A|B|C|D}:NOISe:RN <RN>
Where the {1:8}{A|B|C|D} specifier identifies a module's channel.
Where <RN> is a double.
Query Syntax
:SOURce{1:8}{A|B|C|D}:NOISe:RN?
Description
On simulated modules, specifies the amount of Random Noise (RN) to be added to the indicated source waveform. Enter the value in volts (electrical waveforms) or Watts (optical waveforms). To apply the RN to the waveform, use the :NOISe:STATe command.
Requires FlexDCA revision A.02.00 and above.