:SOURce:PLENgth
Source:
Simulate
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SOURce{1:8}{A|B|C|D}:PLENgth <pattern_length>
Where the {1:8}{A|B|C|D} specifier identifies a module's channel.
Where <pattern_length> is an integer that is the length of the pattern.
Query Syntax
:SOURce{1:8}{A|B|C|D}:PLENgth?
Description
Sets or queries the length of the simulated waveform's pattern in symbols. The simulated waveform's type must be set to data using the :SOURce:WTYPe command. If the waveform type is not set to data, you cannot set the pattern length and the query returns a value of "1" symbol.
To set or query the pattern length for triggering the N1000A on a real input signal, use the :TRIGger:PLENgth command.
Requires FlexDCA revision A.02.00 and above.