:SOURce:JITTer:STATe
Source:
Simulate
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SOURce{1:8}{A|B|C|D}:JITTer:STATe {ON | OFF | 1 | 0}
Where the {1:8}{A|B|C|D} specifier identifies a module's channel.
Query Syntax
:SOURce{1:8}{A|B|C|D}:JITTer:STATe?
Query Response
{1 | 0}
Description
On simulated modules, applies or removes Random Jitter (RJ) to the source waveform. To specify the amount of RJ, use the :SOURce:JITTer:RJ command.
Requires FlexDCA revision A.02.00 and above.
Example Command Sequence
:SOURce2B:JITTer:RJ 1.0E-12 :SOURce2B:JITTer:STATe ON