:SOURce:CDIVide
Source:
AWG
Simulate
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SOURce{1:8}{A|B|C|D}:CDIVide {UNITy}
Where the {1:8}{A|B|C|D} specifier identifies a module's channel.
Query Syntax
:SOURce:CDIVide?
Query Response
{UNIT}
Description
On Arbitrary Waveform Generator (AWG), sets the clock divide ratio.
Requires FlexDCA revision A.06.00 and above.
Selecting AWG Channels
When sending a :SOURce subsystem command to an AWG, the method used to specify the AWG's channel may look confusing at first glance. This is because, the AWG's front-panel channels are labeled 1, 2, 3, and 4, but FlexDCA identifies channels with letters (A, B, C, or D). As a result, you must convert the AWG's channel number to an equivalent FlexDCA letter as shown in this table. For example, to enable channel 3 of an AWG that is installed in FlexDCA's slot 5 use the following command: :SOURce5C:CDIVide UNITy.
| AWG Channel |
Equivalent Letter |
|---|---|
| 1 | A |
| 2 | B |
| 3 | C |
| 4 | D |