:SOURce:JITTer:RJ
Source:
Simulate
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SOURce{1:8}{A|B|C|D}:JITTer:RJ <seconds>
Where the {1:8}{A|B|C|D} specifier identifies a module's channel.
Where <seconds> is a double.
Query Syntax
:SOURce{1:8}{A|B|C|D}:JITTer:RJ?
Description
On simulated modules, specifies the amount of Random Jitter (RJ) to be added to the indicated source waveform. Enter the amount of jitter in seconds. To apply the RJ to the waveform, use the :JITTer:STATe command.
Requires FlexDCA revision A.02.00 and above.
Example Command Sequence
:SOURce2B:JITTer:RJ 1.0E-12 :SOURce2B:JITTer:STATe ON