:SOURce:FUNCtion
Source:
Simulate
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:SOURce{1:8}{A|B|C|D}:FUNCtion {COSine | SINE | SAWTooth | SQUare | TRIangle}
Where the {1:8}{A|B|C|D} specifier identifies a module's channel.
Query Syntax
:SOURce{1:8}{A|B|C|D}:FUNCtion?
Query Response
{COS | SINE | SAWT | SQU | TRI}
Description
On simulated modules, selects a function to create the source waveform. To apply the function to the source waveform, use the :SOURce:WTYPe FUNCtion command.
Requires FlexDCA revision A.02.00 and above.
Example Command Sequence
:SOURce9A:FUNCtion COS