:SPRocess:FFEQualizer:DCGain?
Query Syntax
:SPRocessN:FFEQualizer:DCGain?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Returns the DC gain of a Linear Equalizer operator (LFE).
For Reference Rx operator, what function do I send this command to?
If the FFE (Linear Equalizer) equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:FFEQualizer:DCGain command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:FFEQualizer:DCGain
The Linear Feedforward Equalizer operator is provided with the N1010A-201 Advanced Waveform Analysis license.