:SPRocess:FFEQualizer:NPRecursors

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:FFEQualizer:NPRecursors <precursors>

<precursors> is a int.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:FFEQualizer:NPRecursors?

Description

Specifies precursors for a Linear Equalizer operator (LFE). To enter the number of taps, use the :SPRocess:FFEQualizer:TAPS:COUNt command. Before you can use these commands, turn on the automatic determination of tap values (:SPRocess:FFEQualizer:TAPS:AUTo ON). To manually enter tap values, first disable automatic tap configuration (:SPRocess:FFEQualizer:TAPS:AUTo OFF), then use the :SPRocess:FFEQualizer:TAPS command.

For Reference Rx operator, what function do I send this command to?

If the FFE (Linear Equalizer) equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:FFEQualizer:NPRecursors command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:FFEQualizer:NPRecursors

The Linear Feedforward Equalizer operator is provided with the N1010A-201 Advanced Waveform Analysis license.

Beginning with FlexDCA revision A.05.60, use of an *OPC? query to pause program execution while waiting for this command to execute.

Example Command Sequence

:FUNCtion2:FOPerator FFEQualizer
:SPRocess2:FFEQualizer:TAPS:AUTo ON;*OPC?
:SPRocess2:FFEQualizer:TAPS:COUNt 5;*OPC?
:SPRocess2:FFEQualizer:NPRecursors 3;*OPC?
:SPRocess2:FFEQualizer:TSPacing:TPBit 2
:SPRocess2:FFEQualizer:BANDwidth:AUTo OFF
:SPRocess2:FFEQualizer:BANDwidth 8.0E9
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.