:SPRocess:FFEQualizer:PRESets:SELections?
Query Syntax
:SPRocessN:FFEQualizer:PRESets:SELections?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Response
"preset name, preset name, preset name, …"
Description
Returns a string which is a comma-separated list of all saved presets for the Linear Feedforward Equalizer operator (LFE). Use the PRESet command to load one of these presets.
Linear FFE Operator Presets
- No available Keysight presets.
For Reference Rx operator, what function do I send this command to?
If the FFE (Linear Equalizer) equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:FFEQualizer:PRESets:SELections command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:FFEQualizer:PRESets:SELections
Requires FlexDCA revision A.04.50 and above.