:SPRocess:FFEQualizer:TAPS:LIMits:POST:MAX

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:FFEQualizer:TAPS:LIMits:POST:MAX "tap_value, tap_value, …"

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Where "tap_value, tap_value, …" is a list of doubles. For example, "0.05, 0.20, 0.10, 0.10".

Query Syntax

:SPRocessN:FFEQualizer:TAPS:LIMits:POST:MAX?

Description

For Postcursors, enters a list of maximum allowable values for the Linear Equalizer operator (LFE). To apply your tap limits, use the :SPRocess:FFEQualizer:TAPS:LIMits:STATe command.

For Reference Rx operator, what function do I send this command to?

If the FFE (Linear Equalizer) equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:FFEQualizer:TAPS:LIMits:POST:MAX command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:FFEQualizer:TAPS:LIMits:POST:MAX

The Linear Feedforward Equalizer operator is provided with the N1010A-201 Advanced Waveform Analysis license.

Requires FlexDCA revision A.07.80 and above.