:SPRocess:FFEQualizer:NPRecursors:AUTO
Command Syntax
:SPRocessN:FFEQualizer:NPRecursors:AUTO {ON | OFF}
<precursors> is a int.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:FFEQualizer:NPRecursors:AUTO?
Description
Sets automatic configuration of the Linear Feedforward Equalizer (FFE) operator precursors on or off:
- ON
- Automatic configuration is on, which is the default setting. Use the
:SPRocess:FFEQualizer:MNPRecursorscommand to set or query the maximum number of precursors allowed. - OFF
- Automatic configuration is off. When setting automatic configuration off, follow the command with the
*OPC?query. Use the:SPRocess:FFEQualizer:NPRecursorsparent command to manually set or query the number of precursors for the operator.
For Reference Rx operator, what function do I send this command to?
If the FFE (Linear Equalizer) equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:FFEQualizer:NPRecursors:AUTO command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:FFEQualizer:NPRecursors:AUTO
The Linear Feedforward Equalizer operator is provided with the N1010A-201 Advanced Waveform Analysis license.
Requires FlexDCA revision A.07.80 and above.