:SPRocess:FFEQualizer:PRESets
Command Syntax
:SPRocess:FFEQualizer:PRESets <string>
Description
Loads a previously saved a preset for a Linear Feedforward Equalizer operator (LFE). The preset configures the operator to your saved settings. There are no factory provided presets for this operator. To query which presets are available for loading, use the PRESets:SELections? query.
Linear FFE Operator Presets
- No available Keysight presets.
Presets can only be saved from the operator's Setup dialog. There is no programming command for this task.
For Reference Rx operator, what function do I send this command to?
If the FFE (Linear Equalizer) equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:FFEQualizer:PRESets command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:FFEQualizer:PRESets
Requires FlexDCA revision A.04.50 and above.
Example Command
:SPRocess3:FFEQualizer:PRESets "MyPreset" // Load a saved preset.