:SPRocess:FFEQualizer:TAPS:LIMits:MAIN:MIN
Command Syntax
:SPRocessN:FFEQualizer:TAPS:LIMits:MAIN:MIN "tap_value"
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Where "tap_value" is a double. For example, –0.10.
Query Syntax
:SPRocessN:FFEQualizer:TAPS:LIMits:MAIN:MIN?
Description
Enters a minimum value of the Main tap for the Linear Equalizer operator (LFE). To apply your tap limits, use the :SPRocess:FFEQualizer:TAPS:LIMits:STATe command.
For Reference Rx operator, what function do I send this command to?
If the FFE (Linear Equalizer) equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:FFEQualizer:TAPS:LIMits:MAIN:MIN command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:FFEQualizer:TAPS:LIMits:MAIN:MIN
The Linear Feedforward Equalizer operator is provided with the N1010A-201 Advanced Waveform Analysis license.
Requires FlexDCA revision A.07.80 and above.