:SPRocess:FFEQualizer:TAPS:RECalculate
Command Syntax
:SPRocessN:FFEQualizer:TAPS:RECalculate
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Initiates a re-calculation of the tap values for a Linear Equalizer operator (LFE). Do not follow this command with an *OPC? command. Automatic tap configuration must first be enabled (:SPRocess:FFEQualizer:TAPS:AUTo ON).
For Reference Rx operator, what function do I send this command to?
If the FFE (Linear Equalizer) equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:FFEQualizer:TAPS:RECalculate command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:FFEQualizer:TAPS:RECalculate
Requires FlexDCA revision A.05.60 and above.
The Linear Feedforward Equalizer operator is provided with the N1010A-201 Advanced Waveform Analysis license.