:SPRocess:FFEQualizer:PNOise:BANDwidth:AUTo
Command Syntax
:SPRocessN:FFEQualizer:PNOise:BANDwidth:AUTo {OFF | ON}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:FFEQualizer:PNOise:BANDwidth:AUTo?
Description
Turns on or off the use of automatic bandwidth setting when using noise preservation on a Linear Feedforward Equalizer (LFE). If the setting is off, enter the desired bandwidth using the :BANDwidth parent command. To turn on noise preservation, use the :PNOise parent command.
For Reference Rx operator, what function do I send this command to?
If the FFE (Linear Equalizer) equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:FFEQualizer:PNOise:BANDwidth:AUTo command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:FFEQualizer:PNOise:BANDwidth:AUTo
Requires FlexDCA revision A.05.60 and above.