:SPRocess:RRX:PRESets

Instrument:
N1000A-PLK
N109X-PLK
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:RRX:PRESets <string>

Description

Loads a previously saved a preset for a Reference Rx operator. The preset configures the operator to your saved settings. There are no factory provided presets for this operator. To query which presets are available for loading, use the RRX:PRESets:SELections? query.

What function do I address this command to?

Always address the :SPRocess:RRX:PRESets command to the Reference Rx's output function. In the following figure of the Reference Rx Setup dialog's operator diagram, this would be Function 2. In this case, the command would be:

:SPRocess2:RRX:PRESets "MyPreset"

Ref. Rx Equalizer Presets

  • IEEE 802.3dj Draft 2.3
  • CEI-112G-Linear TP1a (53GBd)
  • CEI-112G-Linear TP4 (53GBd)
  • IEEE 802.3dj Draft 2.0
  • IEEE 802.3bs Amended
  • IEEE 802.3bs
  • IEEE 802.3cd
  • IEEE 802.3db SR SECQ
  • IEEE 802.3db SR (844-863 nm)
  • IEEE 802.3db VR (842-948 nm)
  • IEEE 802.3db VR (842-918 nm)
  • IEEE 802.3db VR (842-888 nm)
  • IEEE 802.3db VR (842-868 nm)
  • Fiber Channel PI - 7 Rev 0.13
  • TDEC ITU 50G PON OLT
  • TDEC ITU 50G PON ONU

Presets can only be saved from the operator's Setup dialog. There is no programming command for this task.

Requires FlexDCA revision A.07.80 and above.

Example Command

:SPRocess3:RRX:PRESets "IEEE 802.3dj Draft 2.3"  //  Load a saved preset.