:SPRocess:RRX:PROPtimize
Command Syntax
:SPRocessN:RRX:PROPtimize {ON | OFF}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RRX:PROPtimize?
Description
For the Reference Rx operator's Non-Linear Equalizer (DFE), turns Pulse Response Optimization on or off. When Pulse Response Optimization is on, you can configure the optimization using these two settings:
- Pulse Delay (Dp)
- The pulse delay can be set from 1 to 10 UIs with the default being 3 UI. Use the
:SPRocess:RRX:PROPtimize:DELaycommand. - Pulse Lengh (Np)
- The pulse length can be set from 9 to 1,000 UIs with the default being 200 UI. Use the
:SPRocess:RRX:PROPtimize:LENGthcommand.
What function do I address this command to?
Always address the :SPRocess:RRX:PROPtimize command to the Reference Rx's output function. In the following figure of the Reference Rx Setup dialog's operator diagram, this would be Function 2. In this case, the command would be:
:SPRocess2:RRX:PROPtimize ON
Requires FlexDCA revision A.07.80 and above.