:SPRocess:RRX:PNOise:BANDwidth:AUTo
Command Syntax
:SPRocessN:RRX:PNOise:BANDwidth:AUTo {OFF | ON}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RRX:PNOise:BANDwidth:AUTo?
Description
Turns on or off the use of automatic bandwidth setting when using noise preservation. If the setting is off, enter the desired bandwidth using the :SPRocess:RRX:PNOise:BANDwidth command. To turn on noise preservation, use the :SPRocess:RRX:PNOise command.
What function do I address this command to?
Always address the :SPRocess:RRX:PNOise:BANDwidth:AUTo command to the Reference Rx's output function. In the following figure of the Reference Rx Setup dialog's operator diagram, this would be Function 2. In this case, the command would be:
:SPRocess2:RRX:PNOise:BANDwidth:AUTo ON
Requires FlexDCA revision A.07.80 and above.