:SPRocess:RRX:SIFunctions
Command Syntax
:SPRocessN:RRX:SIFunctions {ON | OFF}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RRX:SIFunctions?
Description
Shows or hides the Reference Rx operator's secondary functions. This setting is persistent, is not saved in a function preset, and has a default setting of on.
When the setting is turned off:
- Existing secondary function numbers are removed. For new instances of the operator, the function numbers are not assigned until the setting is turned on.
- Secondary Function waveforms cannot be displayed.
- The TDECQ Reference Point can still be placed on the reference points. Refer to the following section for information on reference points.
- The output of the Reference Rx operator is not affected.
| ON | OFF |
|---|---|
|
|
What function do I address this command to?
Always address the :SPRocess:RRX:SIFunctions command to the Reference Rx's output function. In the following figure of the Reference Rx Setup dialog's operator diagram, this would be Function 2. In this case, the command would be:
:SPRocess2:RRX:SIFunctions ON
Requires FlexDCA revision A.07.80 and above.