:SPRocess:RRX:PROPtimize:DELay
Command Syntax
:SPRocessN:RRX:PROPtimize:DELay <UI>
Where <UI> is unit interval expressed as an integer.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RRX:PROPtimize:DELay?
Description
When pulse response optimization (:SPRocess:RRX:PROPtimize) is on, sets the Pulse Delay (Dp) in UI. The default value is 3 UI. The minimum value is 0 UI and the maximum is 10 UI.
What function do I address this command to?
Always address the :SPRocess:RRX:PROPtimize:DELay command to the Reference Rx's output function. In the following figure of the Reference Rx Setup dialog's operator diagram, this would be Function 2. In this case, the command would be:
:SPRocess2:RRX:PROPtimize:DELay 4
Pulse response optimization (:SPRocess:RRX:PROPtimize) must be on to use this command.
Requires FlexDCA revision A.07.80 and above.